10/31/2018 4:48 AM | |
Joined: 9/16/2013 Last visit: 9/14/2024 Posts: 29 Rating: (0) |
Screen 1/4 |
10/31/2018 4:49 AM | |
Joined: 9/16/2013 Last visit: 9/14/2024 Posts: 29 Rating: (0) |
Screen 2/4 |
10/31/2018 4:50 AM | |
Joined: 9/16/2013 Last visit: 9/14/2024 Posts: 29 Rating: (0) |
Screen 3/4 |
10/31/2018 4:50 AM | |
Joined: 9/16/2013 Last visit: 9/14/2024 Posts: 29 Rating: (0) |
Screen 4/4 |
10/31/2018 8:59 AM | |
Joined: 4/3/2008 Last visit: 10/5/2024 Posts: 386 Rating: (16) |
Seems to me you have to consider that the PLC output is the Simotion Input and vice-versa. pigroplc |
11/1/2018 5:27 AM | |
Joined: 9/16/2013 Last visit: 9/14/2024 Posts: 29 Rating: (0) |
See attached screenshot. Have I implemented the data transfer and receive correctly? |
Follow us on