11/5/2018 7:35 PM | |
Joined: 8/7/2017 Last visit: 3/1/2023 Posts: 14 Rating: (0) |
Hello everyone ! Please help me to understand this issue with discrete alarms on HMI. In my HMI (TP 177B 6'' color PN/DP) one fault is 'Thermo Switch Motor' is triggered which causes machine to stop so we reset the machine from push button and just restart, it works fine always. But when i try to see which bit is raising this fault from ladder logic i couldn't find because it is not coming directly in simple logic(at least for me its not simple). Here i am attaching one pic of the HMI discrete alarms along with the trigger address DB7.DBX101.2. When i searched this trigger address in ladder logic i couldn't find it. So i checked DBB101 whcich was written in STL but its not converting to ladder. I have attached picture of both HMI and the DB101 logic. After this it is a dead end for me. In other machines i have checked faults several times which were originating from individuals bits simply but this one is not so simple(atleast for me ) So, how can i find the exact bit from where this alarm is triggered ? Thanks Attachmentalarms_hmi_logic.zip (202 Downloads) |
Last edited by: Targaryen at: 11/5/2018 7:37:23 PM |
|
11/5/2018 8:07 PM | |
Posts: 2826 Rating: (684) |
Where does M138.2 lead you to? |
Last edited by: #dP at: 11/5/2018 8:08:58 PM |
|
11/5/2018 9:04 PM | |
Joined: 9/21/2012 Last visit: 4/19/2024 Posts: 3911 Rating: (443) |
You just found it, the place where the bit is activated. |
Follow us on