11/21/2018 12:03 PM | |
Posts: 80 Rating:
|
Hi, I have followed @bergmanu 's instructions for adding new layers to the image, but I have not been able to add meta-virtualization layer. It gives a parse error in /meta-virtualization/conf/ not a bitbake file. I have added different layers to the image with no problem, do I have to add something more for this specific layer? Thanks in advance. |
11/21/2018 3:37 PM | |
Joined: 12/12/2016 Last visit: 4/8/2024 Posts: 640 Rating:
|
Hello Laura, Are you using the docker branch from jan? Check out this post, from long ago when I was building an image with docker. Maybe it helps. Kind regards! |
Last edited by: Fe_lipe at: 11/21/2018 3:37:31 PM |
|
11/26/2018 3:12 PM | |
Joined: 12/12/2016 Last visit: 4/8/2024 Posts: 640 Rating:
|
Hello Laura, There are too many changes required, so I don't see docker running on 2.2 or upwards in near future. So for now I would suggest: either building an image against krogoth, or using a different solution for deploying docker based applications, like resin.io. Kind regards! |
Follow us on