11/30/2018 1:44 PM | |
Joined: 8/24/2010 Last visit: 5/23/2024 Posts: 30 Rating: (1) |
Hi Smiffy, I tried several solutions but without any success. I want to create the structure of the pointer with a fornat ANY. I want to use a PUT fonction and change the destination adress following some conditions. That's why I need a pointer in order to change automatically the destination. I tried to create a FB and include the PUT function inside. When I include the FB in the OB1, the DB inst is generated but it's impossible to uncheck the "Optimised Data Block". I tried to create a normal DB, uncheck the "Optimised data block" but the format ANY is still not available... Have you got an idea what I can do? TIA PORTAL V14 PLC : ET200SP 1510 ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 12/3/2018 12:51:57 PMNew subject after splitting |
|
12/3/2018 1:57 PM | |
Joined: 8/24/2010 Last visit: 5/23/2024 Posts: 30 Rating: (1) |
It's not possible to uncheck, it's grey. |
12/4/2018 12:05 PM | |
Joined: 9/23/2005 Last visit: 5/29/2024 Posts: 4560 Rating: (701) |
This forum has a very nice search engine. Some outcome after using it you can find below. https://support.industry.siemens.com/tf/ww/en/posts/put-get-example/167 https://support.industry.siemens.com/tf/ww/en/posts/data-type-any-in-scl/ |
Regards, |
|
Follow us on