12/10/2018 7:33 PM | |
Joined: 7/20/2013 Last visit: 7/1/2024 Posts: 20 Rating: (1) |
Dear Experts, i am facing some issues in writing the values to some of my Dosing pumps, my DB is not optimised, basically i need to write 3 Addresses as follows. START/STOP (Holding register 1000, unsigned short), Direction(Holding register 1001, unsigned short), Speed (Holding register 1002, Floating point), I have created a structure in DB 10 as shown in the attached picture, i configured MB master as shown in the picture, But i am getting the following error " 818B Invalid pointer to the local data source/destination: Size not correct " Can anyone support me to identify the mistake i am doing? i have around 20 different components in this modbus network, and i am successfully reading all the values from them, but the writing function is having this problem. Any help would be appreciated Regards Abi ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 12/11/2018 9:13:26 AMNew subject after splitting |
|
Follow us on