12/20/2018 8:17 PM | |
Joined: 7/23/2018 Last visit: 10/26/2023 Posts: 8 Rating: (0) |
I am using ADD Blocks in my program and I am having issues with it incrementing more than once in a cycle. Attached are the function block and add block areas in my program. I want the ADD blocks to update the pointers by 9 only once a cycle so that I can read the data in my registers and then read the next set of data. I interpret the data and move it to a string to be displayed. For some reason the program is only reading the last set of registers and not the ones in between. I cannot use a positive trigger signal check because I don't have anything to set as the program cycles. Does anyone have any ideas?
AttachmentPictures.zip (114 Downloads) |
Follow us on