12/12/2018 11:11 AM | |
Joined: 3/2/2007 Last visit: 9/17/2024 Posts: 935 Rating: (5) |
Kindly, do you know if there are bigger size Shielded Power Cables, similar to the below ? 150 mm2 ? 185 mm2 ? Thank you 6FX5008-1BB12-2AA0 , Power cable sold by the meter type: 6FX5008-1BB12 4x 120 C UL/CSA, DESINA MOTION-CONNECT 500 Type of delivery: Disposable drum Dmax=56.0 mm, Length (m)=100
|
... thank you ... |
|
Follow us on