12/31/2018 3:15 AM | |
Posts: 12 Rating: (0) |
Hello everyone, happy New Year! I have the following questions in using 6SN1118-0NH01-0AA1 analog interface cards. For using one of the drive as spindle axis, I have questions of - How and through which pin I can send spindle run command to the drive? - Through which pin I can get zero speed signal from the interface card? - Through which pin I can get spindle drive alarm signal from the interface card? The machine needs to have spindle orientation stop for tool changing. Questions related to the orientation function are: - How to realize the orientation function? Should I set and switch the drive to closed loop for orientation? - Which parameter should I use for orientation position adjustment? - Through which pin I can send spindle orientation command to the drive? - Through which on I can get spindle orientation finish signal from the interface card? Thanks! ------------------------------------------------------------------------------------------ |
Last edited by: CNC-retrofitter at: 12/31/2018 3:59:24 AMLast edited by: CS Moderator at: 12/31/2018 12:09:53 PMNew subject after splitting |
|
1/3/2019 5:53 AM | |
Joined: 10/17/2007 Last visit: 4/27/2024 Posts: 3974 Rating: (340)
|
Answer your Q's ( I numbered your questions) A1--set to 56/14 A2, A3 --you need read the manual 611U ch. 6.4 Free I/O define --I post the cut page for output you need find pages before and after that page A4,A5,A6 --that depends: solution #1--if your CNC has spindle orientation function then you can use this 611U card to set it in speed control, all other jobs should be set by CNC parameters solution #2--If your CNC no orientation function, --important!! you cannot use this card but use 6SN1118-1NH01-0AA1 card--1NH01 is position control card. then you need program PLC to send orientation command , also you need read chapter 6.x (6.4, maybe 6.5) to find out ter.# and parameters for the function you need.
|
If you like my comments please |
|
Follow us on