8/16/2015 3:30 PM | |
Posts: 139 Rating:
|
Hi, I experienced that waring pop up when FB or FC is already open in ladder or STL and when compliation make via CFC. Know way to clear those logs? Cheers! |
1/28/2019 3:08 PM | |
Joined: 5/3/2017 Last visit: 5/21/2024 Posts: 673 Rating:
|
Hello MicroMan, in my opinion the warning appears because your blocknumber is in the range of numbers that allocated with existing PCS 7 block libraries. Here is a citation from the PCS 7 Compendium Part A - Configuration Guidelines: "The block range of numbers for AS blocks is already allocated for the range from 0 to 2499 by the standard, add-on and sector-specific libraries. The FB range of numbers is therefore divided up as follows:
The numbers in the range from 2500 to 2599 should be used for creating user-defined blocks." With regards |
Last edited by: Heisenberg2 at: 1/28/2019 3:18:20 PM |
|
Follow us on