1/24/2019 4:25 PM | |
Joined: 12/12/2018 Last visit: 7/1/2020 Posts: 34 Rating:
|
helloo! no one can help!! |
Best Regards, |
|
1/28/2019 11:07 AM | |
Joined: 5/3/2017 Last visit: 5/21/2024 Posts: 673 Rating:
|
Hello Wahbi012, welcome to the PCS 7. In PCS 7 is the standard library the Advanced Process Library (APL), there you can find the block "TimerP". The TimerP block is used for delayed forwarding of start or stop actions through the Out output parameter. More Information about the "TimerP" block you can find in the SIMATIC Process Control System PCS 7 Advanced Process Library. with regards |
1/28/2019 4:12 PM | |
Joined: 5/3/2017 Last visit: 5/21/2024 Posts: 673 Rating:
|
Hello Wahbi012, Ti = 4s Time of delay For a graphic representation see PCS 7 Advanced Process Library at section TimerP functions with regards |
1/28/2019 4:42 PM | |
Joined: 12/12/2018 Last visit: 7/1/2020 Posts: 34 Rating:
|
Dear Heisenberg2, Do i have to put variables assigned in the symbol table for the IN, RESET and OUT? |
Best Regards, |
|
1/28/2019 5:08 PM | |
Joined: 12/12/2018 Last visit: 7/1/2020 Posts: 34 Rating:
|
Dear Heisenber2, I am using OB1 and programming with LADDER |
Best Regards, |
|
1/29/2019 7:29 AM | |
Joined: 5/3/2017 Last visit: 5/21/2024 Posts: 673 Rating:
|
Hello Wahbi012, to use OB1 and programming with LADDER is not really PCS 7 like. In PCS 7 you use only the CFC and SFC editor, because a lot of settings specific for PCS 7 will set automatic. For example if you use CFC and the Advanced Process Library after an OS compile the block icons in WinCC will generate automaticly. The best way to start with PCS 7 is with PCS 7 Getting Started. Here are some usefull links to start with PCS 7:
with regards |
This contribution was helpful to
1 thankful Users |
Follow us on