1/29/2019 9:35 PM | |
Posts: 15 Rating:
|
Hi Guys, I have a problem with logging files. Can I make a backup only of the project without the archive files? Because right now the archive file are making the project bigger and bigger and it is almost imposible to manage it. Obviously one solution is put the acquisition cycle larger, but at the end the project will be difficult to make a backup, because it is well know the project has to be closed and I can´t close the project for an entire hour and leave the plant without operation!! Thanks, Luis F. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 1/30/2019 9:48:17 AMNew subject after splitting |
|
Follow us on