1/15/2019 12:21 PM | |
Joined: 3/13/2015 Last visit: 8/27/2024 Posts: 136 Rating:
|
Hi all, I'm trying to build an custom F-block type (Compile CFC as block type) with a standard output. When I create a CFC with F function blocks and add some standard chart IO the compilation works fine. For example a standard BOOL. How do I connect internally a F-output or other logic to the standard outputs? When I add standard blocks (gray) like F_FBO_BO the compiler gives an error because there is safety and non safety within the same program... Hope you can help me! Regard, Cedric Ps. I'm already familiar with the standard documentation on F-systems and the compendium, but did not find any answers. Pps.Find this forum but it does not describe outputs, only an input: datatype-and-f-datatype |
2/5/2019 1:43 PM | |
Joined: 3/13/2015 Last visit: 8/27/2024 Posts: 136 Rating:
|
Thank you for your reply! This can be an workaround, it would be nice to have a block FBO_TO_BO in yellow Regards, |
Follow us on