Industry Online Support
Technical Forum
4/2/2006 8:00 PM | |
Joined: 1/7/2006 Last visit: 11/17/2023 Posts: 2705 Rating:
|
Hi peva, First of all you need STEP5 V7.2x (when you working with a newer Windows Version). [:blush:] The files you mentioned are for: 09.03.1995 14:36 128 2441@@DR.INI Printer 13.01.1997 17:00 640 2441@@F1.INI Header file printer 09.03.1995 14:36 1152 2441@@F2.INI Header file printer 04.01.1995 14:53 6656 2441@@LS.INI Printed file 06.02.1995 23:08 384 2441@@PJ.INI Project file (throw away) 16.03.2000 11:43 277120 2441@@ST.S5D STEP5 file 16.03.2000 11:40 81920 2441@@XR.INI Crossreference file 16.03.2000 11:41 82944 2441@@Z0.INI Symbolik file 20.01.1997 15:06 86656 2441@@Z0.SEQ idem = ASCII 20.01.1997 15:06 39936 2441@@Z1.INI Symbolik fiel 20.01.1997 15:06 9216 2441@@Z2.INI Symbolik file 19.01.1997 15:11 256 2441@@ZF.INI Error file 20.01.1997 15:06 256 2441@@ZF.SEQ Error file 14.11.1995 16:38 256 2441@@ZT.SEQ ?? A link to the STEP5 handbook http://support.automation.siemens.com/WW/view/en/1175533 The data for ordering the STEP5 program you might find in the next link http://support.automation.siemens.com/WW/view/en/9860493 When you have STEP7 then you might convert S5 to S7 to read the program, but a way back is not there. When it is not a big program (277120=big when not comprimaired), then you can say to the customer that you directly migrate... [:P] Best regards, Late |
I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
Follow us on