2/22/2019 1:50 PM | |
Joined: 10/11/2006 Last visit: 11/14/2024 Posts: 5941 Rating: (816)
|
Hello, the fastest cycletime with D455-2 is 125us. 0,125 ms (only with ET 200SP, SCOUT TIA and Servo_fast/IPO_fast). Controller-Drive communication is minimal 0,250 ms. Information: Chapter 6.7.3 https://support.industry.siemens.com/cs/ww/en/view/51786364 Most motioncontrol application with isochronous communication and DSC are running in 2 - 4 ms. It is possible to run servo-fast (0,125 ms) and servo (e.g. 2 ms ) on 1 controller, because fast cycletime cost performance and it makes no sense to calculate everything in a fast cycle. |
With best regards, |
|
Follow us on