2/27/2019 12:24 PM | |
Joined: 10/11/2006 Last visit: 8/7/2024 Posts: 5887 Rating:
|
Hello, an automatic firmware upgrade of the offline device is not possible in Startdrive V15. Here is an FAQ which describes how to do it without deleting and reconfiguring the drives: https://support.industry.siemens.com/cs/ww/en/view/109755173 (please sea chapter 5 in the manual) |
With best regards, |
|
2/27/2019 4:25 PM | |
Posts: 6 Rating:
|
What i should do to upgrade a offline project? The only way to use again starter? Yes two infeed connected on the same line. |
Follow us on