3/6/2019 2:30 PM | |
Joined: 2/28/2013 Last visit: 6/20/2024 Posts: 32 Rating: (0) |
Hello everybody, did anyone find a solution for the described situation from "Milov"? I have a symbol which opens a PopUp when I click on it. The size of the PopUp is not always the same and to do a proper positioning of the PopUp I need to know the size of it before it gets opened. Unfortunately, the size is only set after the PopUp is set to "Visible". Right now I do the positioning afterwards which leads to some kind of ugly flashing on the first opening. Has anyone a good idea how I could solve that "flashing issue"? Can I get the dimensions of a picture somehow before it is actually visible in runtime? Thanks for any help, BR MAB_cc ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 3/7/2019 9:06:52 AMNew subject after splitting |
|
Follow us on