3/13/2019 5:25 AM | |
Joined: 12/18/2014 Last visit: 9/26/2024 Posts: 33840 Rating: (4206) |
Communication Service Packages (CSP) for WinCC im TIA Portal Attached are the latest Communication Service Packages for WinCC in TIA Portal ready for downloading. - Communication Suppport Package for communication via Standard Modbus RTU and Modbus TCP/IP The Communication Service Packages (CSP) will enables you to configure the communication for SIMATIC HMI Panels to PLCs that are not contained in the normal WinCC (TIA Portal) Installation. |
Follow us on