3/15/2019 8:51 PM | |
Joined: 9/2/2012 Last visit: 7/22/2024 Posts: 711 Rating:
|
Hello, Is it done successfully ? I also having similar requirements and going through forum discussion. 1 redundant server pair and few clients. Wincc 7.4 sps upd8 Since it's redundant server architecture, am not sure how to do that. In forum discussion also little bit confuacon. Pls clarify. 1. If I want to keep my wincc-client PC as web server for other business PC, which license is Required ? 2. In case 1, after I assign pck file also, I can't see pdl files while running the web-navigator wizard. Is it normal or am I missing something ? 3. Is there any way to keep redundant server as webserver ? 4. I have read load balancing configuration. It will be applicable if I make redundant server as webserver or client as webserver ? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 3/18/2019 11:17:24 AMNew subject after splitting Last edited by: Jen_Moderator at: 3/18/2019 2:38:45 PMOptimized headline.
|
|
This contribution was helpful to
1 thankful Users |
Follow us on