3/28/2019 3:36 PM | |
Joined: 10/11/2006 Last visit: 7/10/2024 Posts: 5872 Rating: (797)
|
Hello Skander, there is a SIMATIC block available to read out drive parameters acyclically. They are called SINA_PARA or SINA_PARA_S. (the difference between these two is with SINA_PARA_S you only can read/write one drive parameter, with the other one you can read/write multiple drive parameters). Please have a look at the following SIOS entry: https://support.industry.siemens.com/cs/ww/en/view/109475044 |
With best regards, |
|
This contribution was helpful to1 thankful Users |
Follow us on