1/24/2013 8:48 PM | |
Joined: 1/23/2013 Last visit: 10/17/2024 Posts: 38 Rating: (1) |
When we make update from V7.1+SP3 to V8 we have to change all CH_DI block into PCS7DiIT( and other CH_DO,CD_AI). |
4/11/2019 3:11 PM | |
Joined: 6/26/2018 Last visit: 10/11/2024 Posts: 43 Rating: (0) |
Hello Everyone
l sent logs and what l did to you in attachment. Normally other engineer never use PCS7 AP V.8.2 Library in my company. But l insert new chart then l use 1 valve block and 2 CH_DI in this chart. when l compile , compile has a error. then l delete this chart with valve and 2 digital input block. l try again but compile error still exist. Error say :Necessary files are missing for [ block CH_AI ] please note that you have to install exactly the same version of the library as the one this block was imported from. After , l searched all chart for find CH_AI from AP V.8.2 Library. but l never find CH_AI block from AP V8.2 library in all chart. l look simens support and read all advise . so l did one this thats l sent you in attachment. you can see Error photo and what l did. Best Regards AttachmentLogs and what l did.zip (198 Downloads) |
4/11/2019 5:38 PM | |
Joined: 9/9/2015 Last visit: 10/10/2024 Posts: 728 Rating: (279) |
Dear YellowBeard, Is okay to use APL Library, nothing wrong with it. As long as the FB number didnt crash with your current one, it will be fine. However, you must do one thing, to install the library. There is a installer to installer all the required module driver files and registry in to your system drive. So now, you need to clean the block from the chart database. When you move a block from library to your folder, you are moving a block into your offline block folder as well as the chart database/folder. When you delete it from the chart, the block is still exist in your offline block folder. The proper way to clean it is, go to CFC editor-> option -> block type-> Clean up read the instruction, clean the FB that is causing the error. Then it will be fine. |
Please give me 5 stars Rating if my post is helpful for you. :) |
|
This contribution was helpful to1 thankful Users |
Follow us on