4/11/2019 9:44 AM | |
Joined: 8/3/2009 Last visit: 4/30/2024 Posts: 12869 Rating: (1643) |
Hello tmduy99 Check also if a Ping works from your Engineering PC to the PLC. you also can use the Automation tool (LINK) or Proneta (LINK) to define the IP Adress of Profinet Devices. Bye Murof |
If this Information really helps, you could use the Rate function |
|
4/12/2019 9:05 AM | |
Posts: 3 Rating: (0) |
Thanks for help, but it is not my problem, my IP address is 192.168.0.3 |
4/12/2019 9:08 AM | |
Posts: 3 Rating: (0) |
tkanks for help, but i still can't connect to PLC, the ping work is normal |
4/12/2019 9:12 AM | |
Posts: 1283 Rating: (105) |
can you try to disbale your wireless netw adapter and using LAN cable for direct connection to PLC and try again? |
4/12/2019 11:26 AM | |
Joined: 8/31/2005 Last visit: 4/26/2024 Posts: 2197 Rating: (326) |
Check this FAQ, https://support.industry.siemens.com/cs/ww/en/view/109762832 Do you have somethink similar installed or do you use a switch or router ? |
|
|
Follow us on