4/11/2019 10:34 AM | |
Posts: 17 Rating: (0) |
I am trying to get signals on PLC from Emergency Stops and not sure why I can't. I get the signals in the Profinet DI module and it is working without faults0 but I can't see anything on PLC when I watch them. When any of EStops gets pressed, the Profisafe DI module goes to fault (SF LEDs is red and at the ET200S too). Sorry for my ignorance, but it is first time I work with this and I am not sure if I need to do another procedure with the code to read the tags and configurate the modules. I am working with an S7-1511 F and ET200S and Profisafe 4/8 F-DI DC24V_1 Thanks. AttachmentProfiSafe.zip (185 Downloads) |
4/11/2019 6:36 PM | |
Joined: 9/21/2012 Last visit: 7/29/2024 Posts: 4050 Rating: (456) |
Just to be clear, can you please show us a diagram how the connections are made? |
Follow us on