5/2/2019 10:13 AM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating:
|
hi, Simatic Net should be a content of the SW where it is needed. I would try to use the download of the Step7 professional 2010 SP4 May it can be fixed with this Service Pack hope this helps, regards, |
FCK WAR! |
|
5/2/2019 1:07 PM | |
Joined: 9/30/2016 Last visit: 7/11/2024 Posts: 914 Rating:
|
Thank you for answering mopS04. According to the CD cover Step7 professional 2010 SP4 is already included in the Step 7 Pro 2010 SR4 CD I used to install from. I think I did a search for the file on the CD - but I guess it might be packed in some form or other. Still - it would be nice to get the correct file.
|
5/2/2019 2:24 PM | |
Joined: 9/30/2016 Last visit: 7/11/2024 Posts: 914 Rating:
|
Thank you for answering ChristophD, Unfortunately the screenshots I made have been deleted - but it said as I wrote in my original post. You are however also right that something WAS wrong. I had installed Step 7 V5.6 together with WinCC 7.0 SP3 Upd1 (and Step 7 Safety V5.4 and TIA V15 and could not get WinCC to work - I was told that I needed an older Step 7 to make it work - see thread https://support.industry.siemens.com/tf/ww/en/posts/how-do-i-fix-project-manager-for-configured-wincc-server-is-not-already-running/212644/?page=0&pageSize=10 So I uninstalled all the SW from Siemens with the Windows feature "Uninstall Programs" and tried installing the older versions. I had feared all along that Siemens are installing the programs so sloppy that they are almost impossible to uninstall cleanly. So I am going to start with a fresh install of Win7 now - even though it shouldn't be necessary.
|
Follow us on