5/16/2019 2:23 PM | |
Joined: 12/12/2016 Last visit: 4/8/2024 Posts: 640 Rating: (60)
|
Hello, 1) Yes, you can e.g store data in files (CSV, TXT, XML...) on the filesystem of the IOT2040 2) We don't have any application examples for OPC Classic. Only OPC UA. But you can check out the different available toolkits on here. There are definately some cross-plattform solutions such as OpenOPC. So you will have to try them to find out. 3) See answer above 4) Fanuc has various different machines. It depends on what communication protocols the machine supports. Modbus-TCP could be an option. Kind regards! |
Follow us on