5/28/2019 11:48 AM | |
Joined: 4/24/2019 Last visit: 1/10/2022 Posts: 6 Rating:
|
Hello there, I am currently trying to access a SIMOTION C240 PN. The goal is to program a test interface for which I need to access and read a Variable on the Device. I thought about using Snap7 as I did before with other Siemens PLC's but it seems like Simotion has a different architecture. I also tried to figure out the address of certain variables in the memory (e.g. DB) in the Simotion Scout like it was mentioned in another topic (https://support.industry.siemens.com/tf/ww/en/posts/simotion-d4x5-connecting/180144?page=0&pageSize=10) but there is no such information?! I'd be thankful for every input on that issue. Best regards, Simon
|
5/28/2019 12:01 PM | |
Joined: 5/12/2006 Last visit: 7/9/2024 Posts: 22304 Rating:
|
Hello, which information exactly? Christoph |
Follow us on