5/23/2019 10:47 AM | |
Joined: 11/14/2018 Last visit: 7/26/2024 Posts: 502 Rating: (69) |
Hello Sachinpatke, you are right, since V14 the Sm@rtSever license is included, you don't have to get an extra licencse. For sending an SMS (via E-mail), in the runtime settings you have to configure the "SMTP communication" settings to the SMTP server you want to use. Which SMTP server you choose is up to you, because the SMTP server itself is not provided by WinCC. I hope this helps, Greetings, Nzett11 |
If I could help you, be so kind and rate my contribution. :) |
|
Follow us on