5/30/2019 6:58 AM | |
Joined: 12/9/2010 Last visit: 10/8/2022 Posts: 623 Rating: (76) |
Hi Nikodem93, What do u mean by 'Loop of data'. As there is no processing on data in loop, nothing will happen to string. Only variable 'Point_to' will be incremented. Note 'count' should be divided by 10 or should be given fixed value. |
If you like the comment, rate it (right top) or thank it (left bottom). |
|
6/1/2019 2:11 PM | |
Joined: 12/9/2010 Last visit: 10/8/2022 Posts: 623 Rating: (76) |
Hi Nikodem93, If u have fixed length of number of strings ( or queue) (say 20), then there is simple solution with SFC20 (BLK_MOV). Logic- If there is positive edge, initially move string 1 to 19 to string 2 to 20 addresses. Then move new data to string 1 position. Hope this works!!! |
If you like the comment, rate it (right top) or thank it (left bottom). |
|
Follow us on