6/7/2019 9:05 AM | |
Joined: 11/7/2011 Last visit: 1/27/2023 Posts: 96 Rating: (0) |
DEAR ALL, I NEED TO CONTROL 6RA80 FROM ALLEN-BRADLEY PLC OVER PROFIBUS.WHAT PARAMETERS ,I NEED TO SET IN DRIVE FOR SPEED REFERENCE START/STOP,ACTUAL CURRENT,FIELD FAULT ETC. CAN ANYBODY TELL ME THE PARAMETERS OF DRIVE ,WHICH I NEED TO SET OR PROGRAM. THANKS & REGARDS, SAMIR ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 06/07/2019 12:53:59New subject after splitting |
|
6/7/2019 7:31 PM | |
Joined: 11/7/2011 Last visit: 1/27/2023 Posts: 96 Rating: (0) |
DEAR SIR, I KNOW PLC PROGRAMMING,I WANT TO KNOW DRIVE PARAMATERS TO BE SET IN DRIVE FOR OPERATING DRIVE OVER PROFIBUS. |
6/8/2019 7:07 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (872) |
Hello, Please refer attached files, having information of internal control & status words & profibus send & receive telegram information. HTH. Attachment6RA80 profibus communication .zip (92 Downloads) |
Follow us on