6/12/2019 8:03 PM | |
Posts: 7 Rating: (0) |
I am trying to download one of our Simotion D435 motion control CPU's with a slightly changed user program to make the machine run slightly different. We have 2 of these production lines and I downloaded the other one with no issues. I have also downloaded this one in the past to make changes and had no issues. I thought I was having a corrupted program issue so I reverted back to an older program that I know i had downloaded the drive controller with. It still has the same faults. I put a support ticket in and they recommended updating the firmware to 4.1.5.15. This I did and still the same faults. I am using a Scout 4.3 & 4.2 both versions with both firmware's of 4.1.5.6 and 4.1.5.15 result in the same errors. I have attached the device diagnostics to review that also has the device characteristics and everything, Also sometimes i download and all red lights flash and I have to power cycle the unit to revert back to the old program to make it run again. It is weird that I can compile the CPU on the laptop and everything completes fine with only a couple warnings but then when I download it claims inconsistencies. I have also tried many different versions of the TP_CAM technology package but every time i try to over-write the old version of technology packages via checkbox in download options the download fails. I have tried to move it up to v4.1.5.15 and also tried reverting back to an earlier version. I know this device diagnostics was from before I downloaded the firmware but the new firmware did not appear to change anything anf had the same faults at the same time in the same way. AttachmentDiagnostic buffer.txt (168 Downloads) |
6/12/2019 8:13 PM | |
Posts: 7 Rating: (0) |
I will attached the 2nd log file if anybody wants to take a stab at what the actual problem is. |
Follow us on