6/12/2019 2:46 PM | |
Joined: 8/22/2016 Last visit: 7/29/2024 Posts: 37 Rating: (8) |
Hello guys, I have similar problem and I really found out, that with the OPC client UA expert, there is everything like I expect. However with my OPC client, which I wrote based on the Siemens example, there are no variables in the tree visible, while I try to explore the server's content. PLC is S71500 family (I tried 1510, and 1516) with firmware 2.6. With older firmware 2.1 was everything OK. Probably downgrade of firmware wold solve the problem, but I don't want to do it forever.
Don't you know if there is any way, how can I update the OPC client application in order to make it together with newer PLC firmwares? I'm thinking for example about update of Opc.Ua.Client.dll ... Regards Josef ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 06/14/2019 09:07:51New subject after splitting |
|
6/24/2019 3:41 PM | |
Joined: 10/10/2005 Last visit: 7/24/2024 Posts: 1917 Rating: (136) |
Hello JBee, I’m not sure but this problem could be solved with the update 2 of STEP 7 (TIA Portal) V15.1. After installation save and compile complete the program and repeat the download. Use the link in refer to download the update: With best regards |
Follow us on