6/24/2019 2:40 PM | |
Joined: 4/14/2010 Last visit: 8/6/2024 Posts: 525 Rating: (11) |
Thank You! AutoGen, This is Servo driven intermittent motion vertical form-fill-seal bagmaker machine. Full servo motor control of all 04 following motion axis (0--100mm) 1. Pull Belt System (Left, Right 02 Axis) 2. Jaw Seal Actuation 3. Stripping Motion Four 200VAC motors are used, One is used to open and close the sealing jaws. The jaw servo motors is mounted at the rear of the jaw carriage. The second strip servo motor is located at front of the machine (attached) mounted on frame. The 3rd and 4th servo motors are used for the drive pull belts. These belts advanced the film are mounted behind the pull belts.
AttachmentMachine Layout.zip (328 Downloads) |
MS |
|
6/25/2019 2:25 PM | |
Joined: 4/14/2010 Last visit: 8/6/2024 Posts: 525 Rating: (11) |
Thank You! OlafS1, In machine manual information there is mention Servo driven intermittent motion 4 axis control. Have a look on attached machine operation, Is it possible without T-CPU.
Attachmentrecord.zip (374 Downloads) |
Last edited by: MS1981 at: 06/25/2019 14:26:17MS |
|
Follow us on