6/11/2019 9:46 AM | |
Joined: 10/12/2017 Last visit: 7/1/2019 Posts: 2 Rating: (0) |
Hi, I can't download project from SINAMICS because of a similiar issue. During the finding an accessible device I got the message "Error occured while determining the accissible nodes (life list)." Do you know what I should do with this? I use ethernet conections via LAN cable. I tried to ping IP adress and it was successful, but when I use Starter so I can't connect. ------------------------------------------------------------------------------------------ |
Last edited by: S_Moderator at: 06/26/2019 12:46:31New subject after splitting |
|
6/11/2019 1:22 PM | |
Joined: 10/12/2017 Last visit: 7/1/2019 Posts: 2 Rating: (0) |
In attachment you see what I have configured. When I use accessible nodes the Simatics is showed, but i can't chose it and click on the accept. Thank you a lot for your help. I am beginer in Starter topic. AttachmentPG_PC_and_accessible_nodes.zip (334 Downloads) |
Follow us on