6/23/2019 5:08 PM | |
Joined: 11/26/2006 Last visit: 10/1/2024 Posts: 36 Rating: (5) |
Hello All, Can someone explain how control card 6sn1118-0nh01-0aa1 detect in which power section is inserted? I am using universal card 6sn1118-0nh01-0aa1 and Simocom V14 for test purposes, and have similar problem with many power sections. In fact. If these power sections are using with different control card ,there is no problem. For example - universal card is inserted in power section 6sn1124-1aa00-0ea1 mand there is alarm a039,2000h.Same power section work normally with 6sn1118-0dg23-0aa0 on the real machine. And there is two question - How control card detect power section, Can I disable this automatic detection for test purproses ? Thank You, Alexander ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 06/24/2019 14:23:13New subject after splitting |
|
Follow us on