7/24/2019 10:35 AM | |
Posts: 25 Rating:
|
Dear Gentlemen, I worked in project using redundant CPUs 6ES7 412-5HK06-0AB0 and We will connect to 3rd party DCS using Modbus TCP, I used Simatic Modbus TCP Wizard to establish Modbus configuration in my Project but after finish wizard it add only 3 DBs, I saw before another project using the same CPUs connect to DCS through Modubs TCP, there were certain Function Blocks and certain STL code in OB1, I don't know wizard can add all these Function blocks and STL code or I have to add it by my self. I attached below item to simplify my question :- 1- Pics show step by step what I did on Simatic Modbus TCP Wizard. 2- Simatic manager project what I did and result of what I make on the wizard. 3- Picture of HW configuration. 4- Picture of Function Blocks used on old project. 5- Pictures of STL Code in OB1 in old Project. Thanks in advance
AttachmentAttachment.zip (384 Downloads) |
Follow us on