8/5/2019 11:49 AM | |
Joined: 7/27/2016 Last visit: 8/29/2024 Posts: 50 Rating: (0) |
Dear All, During Normal running we got the Process Historian Alarm in Operator station but there is no Alarm in system alarms .on checking found the following Errors in Windows Server console Error 10 and Error 7022. Photos attached in attachment. PLEASE SUGGEST SOLUTION.... THANKS '...
AttachmentPH ERROR.zip (87 Downloads) |
8/6/2019 10:01 AM | |
Joined: 9/9/2015 Last visit: 9/4/2024 Posts: 727 Rating: (278) |
Dear Hamee, Any other information you can find? Below are additional logs files used for troubleshooting. I also attached an useful information on the operating state on the OS for your reference, do read it carefully. Here attached with the Link for the attached reference. Process Historian 2014 SP3 03/2019 The following log files are available for diagnosing PH, IS and PH Ready. Some of these log files are available in the “ProgramData” directory. This directory path must be displayed in the Windows Explorer. Process Historian C:\ProgramData\Siemens\Logs\ProcessHistorianUI.diagnostic.log C:\ProgramData\Siemens\Logs\Processhistorian.diagnostic.log C:\ProgramData\Siemens\Logs\MaintenanceServer.diagnostic.log C:\ProgramData\Siemens\Logs\DiscoveryService.diagnostic.log Information Server The IS log files are available on the IS in directory C:\ProgramData\Siemens\Automation\Logfiles C:\Program Files (x86)\SIEMENS\InformationServer\log PH-Ready on the WinCC server The PH Ready log files are located on the WinCC server in directory C:\ProgramData\Siemens\Logs\ProcessHistorian. PH SQL server C:\Programs\Microsoft SQL Server\MSSQL10_50.HISTORIAN\MSSQL\Log IS SQL server C:\Programs\Microsoft SQL Server\MSSQL10_50.INFSERVER\MSSQL\Log AttachmentInformationAboutOperatingStateOnTheOS_PG168_172.pdf (97 Downloads) |
Please give me 5 stars Rating if my post is helpful for you. :) |
|
Follow us on