8/7/2019 8:01 AM | |
Joined: 5/6/2010 Last visit: 8/5/2024 Posts: 1975 Rating:
|
Hello WoodyWu, which PLC do you want to download? For a 1200er is a Basic version (6ES7822-0AA05-0YA5) enough. If you need the software for a 1500, then it's the right one. regards |
8/7/2019 8:04 AM | |
Joined: 7/9/2015 Last visit: 8/7/2024 Posts: 3915 Rating:
|
Hi, the question ist, which PLC do you use and do you only want to download HW-Config or do you want to edit it. If you use S7-1200/S7-1500 you can also use Simatic Automation Tool Licenses can be use on one PC and you can MOVE it to another with Automation License Manager.License Keys can also be put on a server. Information about License: https://support.industry.siemens.com/cs/de/en/view/57775228 Regards, Towome |
Last edited by: Towome at: 08/07/2019 08:11:39
|
|
8/8/2019 9:20 AM | |||
Joined: 9/21/2012 Last visit: 8/7/2024 Posts: 4079 Rating:
|
The first one is a Combo license, that covers TIA Portal and Simatic Manager (Classic Step7) The second one is only for TIA Portal. |
||
Last edited by: Hati at: 08/08/2019 16:56:34typo |
|||
This contribution was helpful to
1 thankful Users |
Follow us on