Industry Online Support
Technical Forum
8/8/2019 11:11 AM | |
Joined: 9/17/2011 Last visit: 12/22/2020 Posts: 17 Rating: (0) |
hello Experts, I encountered a tricky problem when I used this sizer tool to select and found that the motor used in my factory but we could not be selected it in sizer because out of the thermal utilization (119.2%) so i want to modify the thermal utilization value to 120% how to do it? And I found in my install path: C:\Users\admin\AppData\Roaming\Siemens\SIZER\xml\SizerSettingsV3_18.xml <SizerAttribute Comment="" Name="GlobStg_Default_Thermische_Ausnutzung" Value="#DW1_0x00000000_DW2_0x40590000_100.000000" I modify this value to 120.0 But I have an alarm: internal error This is because of the CRC check I think! So how to modify this and help me to choose the right motor, thank you!
Attachmentsizer.zip (306 Downloads) |
Follow us on