7/16/2019 2:19 PM | |
Joined: 2/12/2015 Last visit: 6/25/2024 Posts: 3 Rating:
|
Hi everyone I have been following this forum for a long time but I find myself writing for the first time just now. I have a problem related to the simatic batch in a dcs on which PCS7 8.0 SP1 is installed with WINCC 7.2 as supervision and Simatic BATCH 8.0 SP1. some premise ... this system was born in 2012 and now has been "redesigned" to the software level and expanded so that from a network closed on itself, everything was on the plant bus, now it has been moved to more pieces of network for which there is a plant bus, a bus terminal and a customer establishment network. the system currently consists of a PLC (CPU416-3) with all its field network, installed in the plant bus (192.168.4.xxx), a communication CP (CP443), installed in the bus terminal (192.168.y. xxx), which is connected to a server network card, and a customer network (10.xxx) to which clients are connected in the corporate domain connected to the server's second network card, so that the server acts as a bridge between the plc, through the cp, and the clients on the plant network, all connected through the Simatic Logon that centralizes the accesses. this is the current project configuration! This displacement, with all the various tests in this regard, has ensured that at present it is possible to correctly compile and download the plc, server and client for OS part of course, and the batch, but after downloading it when you run the Process Cell update inside the Batch Control Center, BCC, the system displays the error in photo1. This means that if I were to implement new functions in the batch I can't do it because it's not possible to update it even if the batch is fully functional. I have tried, here on the forum, solutions in this regard and I have found a procedure, even an official one, which says to delete the batch project on the batch server, in the sbdata folder, and to regenerate the whole project completely re-loading the batch software. I made the attempt but I realized the second mistake. probably the only error, which is represented by photo 2. when I regenerate the batch project, I no longer download the batch database server, so I no longer download the online and offline folders and the project folder. have any of you already faced a similar problem? I hope I was clear in explaining the problem. thank you for every answer or help you give me Hello
Attachmentphotos.zip (117 Downloads) |
Follow us on