8/14/2019 10:40 AM | |
Posts: 6 Rating: (1) |
Hello, Reverting back to the expert circle once again for their help! I have to program for the first time two Sew movitrac B speed variator under TIA Portal V13 Service pack 2 in profinet. I installed the GSDML available on their website, I also added two drives on the network of my Siemens S7-1511PN controller. That is to say, I will just need to start and stop the motor and generate the discrepancy with the motor start up feedback. I also send a speed setpoint from my supervision. I have used the DPRD and DPWR blocks in the TIA portal with the address of the DFE32B modules(profinet gateway for the drive module) for the input LADDR of the block. I also see in my configuration that the words IW308 to IW313 are reserved as inputs and QW288 to QW293 are reserved as outputs by the DFE32B module. I have found some sample projets on the manufacturers website but all are in TIA Portal V14 and not readable by my TIA portal version 13 SP2. Thanks a lot! AttachmentConfiguration.pdf (168 Downloads) |
Last edited by: provat281973 at: 08/14/2019 10:41:42 |
|
Follow us on