8/16/2019 3:46 PM | |
Joined: 9/27/2006 Last visit: 4/27/2024 Posts: 12257 Rating: (2665) |
Hello elityy; There are many, many websites that compare Siemens and Rockwell controllers, most of the critics you can find there pull towards the system they are familiar with and decry the other because of the unfamiliarity. The simplest way for you to begint with a new system is to start with some basic training, which Siemens provides with different media, and working with the programming tools provided. First, the newest software available in Siemens world is TIA Portal, now at v15.1. You can download a demo (trial license) version in the following link. TIA Portal is built on 2 seperate platforms, Step 7 to program the PLCs and WinCC to program the HMI panels/SCADA systems: SIMATIC STEP 7 and WinCC V15.1 TRIAL Download https://support.industry.siemens.com/cs/us/en/view/109761045 As far as project level is concerned, MicroLogix nd CompactLogix should correspond to the power of the S7-1200 family of processors, and the ControlLogix should be equivalent to the S7-1500 family.S7-300 and S7-400 PLCs are still in use and very powerful, but they will eventually be replaced by the S7-1x00 controllers. And to top off this first introduction, here are the promised tutorials: Siemens SCE tutorials, S7-1200 The TIA Portal Tutorial Center (videos) https://support.industry.siemens.com/cs/ww/en/view/106656707 Finally the forum gives you access to many, many manuals, FAQs, Application examples, that you can locate using the search box at the right of this pâge. Use search terms such as TIA POrtal, Step 7 v15, S7-1200... and use the different selections in the Search area to limit thee search range. Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 08/16/2019 15:48:04 |
|
Follow us on