8/22/2019 9:23 AM | |
Posts: 6 Rating: (0) |
Dear Friend, I have one doubt. In VlvL Status Word 1 Bit no 20 - Display „Forced close“ Bit No 21 - Force Bit No 22 - Automatic Preview ( 1 = "Open") Index 0 - No Picture Index 1 - apl_bi_forced.emf Index 2 - apl_bi_bypassed.emf ........ Index 15 If I want to display the Index 8 picture. What should be the value of Status one word Bit No? Thanks, Lakshmanan ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 08/22/2019 13:01:14New subject after splitting |
|
8/28/2019 10:40 AM | |
Joined: 5/3/2017 Last visit: 5/21/2024 Posts: 673 Rating: (217) |
Hello laxman_1985, the VlvL blockicon uses the extended status display to show different symbols. For the picture of index 8 you have to set the bit 3 to TRUE and the bits 0 up to 2 to 0 FALSE. The complete table with the different bits to the index I have attached. More information about the extended status display you can found in the FAQ How do you use and configure an extended status display with SIMATIC PCS 7?. With regards |
Follow us on