8/29/2019 6:15 PM | |
Posts: 9 Rating:
|
Hello I have been told I need to set the password complexity setting on the iot2040 so that it complies with company password policies. All the methods I know to do so rely on pam (if there are any others please let me know I am creating a custom layer and I need to enable pam support before I include a recipe that depends on pam. Apparently I must add, (according to the error I get if I try to include libpam recipe for example)
to the build/conf/local.conf file. I have not had success with this, but since I don't really know what I am doing, I don't really know if I am doing it right. I have found this Yocto wiki entry but I am not sure how to do the necessary things it recommends or if it is still current as it talks about Yocto 1.1. Does anyone have experience of enabling pam support? Alternatively is there is an easier way to check password complexity? EDIT In case anyone is interested in this in the future. I have fixed this simply by adding DISTRO_FEATURES_append += " pam" into the local.conf file in my custom layer. Everything works fine that I can see. |
Last edited by: AutoGen_6692584 at: 08/30/2019 17:42:19Last edited by: AutoGen_6692584 at: 09/02/2019 18:00:10 |
|
Follow us on