9/6/2019 1:01 AM | |
Joined: 9/27/2006 Last visit: 10/17/2024 Posts: 12289 Rating: (2687) |
Hello David; There are ET 200S standalone CPUs, the IM 151-7 (with Profibus slave interface) and IM 151-8 (with integrated Profinet and Profibus master interfaces). Here is the manual for the IM 151-8 to give you pointers, there is one for the IM 151-7 as well. SIMATIC ET 200S distributed I/O IM 151-8 PN/DP CPU interface module https://support.industry.siemens.com/cs/ww/en/view/47409312 Note that there are also ET 200S F-CPUs is you have a Safety program you need to run. The 6ES7151-8FB01-0AB0,ET 200S, IM151-8F PN/DP CPU, 256KB is one possibility. If the S7-1500 is not part of your search parameters, the ET 200SP CPUs (built upon the S7-1500 platform), such as the ones shown in the following link would only be for information Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 09/06/2019 01:07:26 |
|
This contribution was helpful to1 thankful Users |
Follow us on