(0)| 9/6/2019 9:54 PM | |
|
Posts: 57 Rating:
|
After applying the example mentioned inside the main Modbus library And adjust the values compatible with the inverter Have been contacted? Second, how do I determine the memory responsible for sending the engine speed frequency, for example to the inverter And another memory to read the value of the inverter SP: The example applied is the same as the one on page 12 In the attached file
Attachmentdoc_using_modbus_mp_library_en.pdf (817 Downloads) |
Follow us on