9/15/2019 12:35 PM | |
Joined: 1/9/2016 Last visit: 11/9/2023 Posts: 12 Rating: (0) |
Hi everybody. I´m completely new in this forum, but I need to know if there is any example of use for the s210 by stardrive v14 or TIA PORTAL v14. I´m trying to configure one of this system from tia portsal v14 SP1 and i can´t find any s210 to include in my proyect. Is it maybe due to the fact that s210 drivers are included only since the stardrive v15 version o they are available for the v14 version too? Thanks a lot for your attention. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 09/16/2019 12:54:32New subject after splitting |
|
9/16/2019 7:47 AM | |
Joined: 5/12/2006 Last visit: 4/30/2024 Posts: 22243 Rating: (2981) |
hello, not available for TIA / STARTDRIVE V14.
Christoph |
9/16/2019 1:37 PM | |
Joined: 2/7/2018 Last visit: 3/14/2023 Posts: 181 Rating: (30) |
Hi, The Information about the compatibility of SINAMICS S210 and TIA V14 (and also Link to GSDML-Files) can be read in the FAQ below. https://support.industry.siemens.com/cs/ww/en/view/109761460 Best Regards, |
9/23/2019 9:53 AM | |
Joined: 4/28/2015 Last visit: 9/20/2022 Posts: 1278 Rating: (295) |
Hi, I think you need to use version V15.1 - with that the S210 is integrated for sure! |
Best regards, |
|
9/23/2019 10:34 AM | |
Joined: 2/7/2018 Last visit: 3/14/2023 Posts: 181 Rating: (30) |
Hi, Since TIA STARTDRIVE Version V15.1 and SINAMICS S210 Runtime Version V5.2 the SINAMICS S210 is fully integrated in TIA. More information about Startdrive V15.1 and the download can be found here: Available firmware versions for the SINAMICS S210 drive system: https://support.industry.siemens.com/cs/ww/en/view/109744577 Best Regards, |
Follow us on