10/7/2019 1:00 PM | |
Joined: 1/23/2013 Last visit: 8/10/2022 Posts: 226 Rating: (5) |
Hello I could not test D425 v4.3
|
10/8/2019 10:14 AM | |
Joined: 10/11/2006 Last visit: 11/14/2024 Posts: 5941 Rating: (816)
|
Hello that's correct, SIMOSIM support SIMOTION D425 -D455-2 up to version SCOUT V5.1 With each installation SIMOSIM for the same Runtime will be installed. If needed other versions in case of working with SCOU V5.3 on a project Version V5.1 it is possible to install SIMOSIM V5.1 too. Link download SIMOTION SW: https://support.industry.siemens.com/cs/ww/en/view/109480700 Please note: it is also possible to simulate ET200 SP (I/O) |
With best regards, |
|
Follow us on