Industry Online Support
Technical Forum
10/10/2019 3:44 AM | |
Joined: 4/9/2019 Last visit: 4/26/2024 Posts: 2 Rating: (0) |
I'm using SICK ENCODER (ATM60-A1A0-K19 SSI ENCODER), connected to TM PosInput SSI card (6ES7-138-6BA00-OBA0). When using TM PosInput SSI card (from siemens manual for this card iI can see that if bit 0 get enabled on byte 8, it will load value to the encoder (bytes 0…3 loaded value), but every time when I do this bit 2 from byte 12 get active (Error when loading via control interface). Do you have any suggestions on what to do regardings this preset value? P.S. My encoder feedback is perfectly fine (I receive pulses and everything), but I can't preset value. Best regards, ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 10/10/2019 13:29:09New subject after splitting |
|
10/10/2019 1:29 PM | |
Joined: 8/21/2014 Last visit: 4/26/2024 Posts: 950 Rating: (13) |
Closed because question was posted twice. Please use: preset value problem |
My Forum is the place to personalize your profile, |
|
Follow us on