Industry Online Support
Technical Forum
11/1/2008 6:50 PM | |
Posts: 20 Rating:
|
hello Mr. Karl. i attach the dumps from the stoped PLC. the Two plc have db's in the user eprom module. please tell me if need more info thanks Juanjo AttachmentSTOPED.zip (230 Downloads) |
11/1/2008 8:48 PM | |
Posts: 20 Rating:
|
Hello Mr. Karl. the dump sent is of the PLC with Dont running. the eprom if this PLC1 have DBs. (48,49, 59..63, 70...75,80....84,87) the eprom of the PLC2 also have DBs. i attach both programs, thanks Juanjo AttachmentPLCprog.zip (244 Downloads) |
11/2/2008 1:09 PM | |
Posts: 20 Rating:
|
Hello again. i attach the dumps from booth plcs without the user program inserted, only the upper sockets are inserted. the eproms are the original ones (come with the machine), also have copies programed by me, but with the same results. After a review of the listing, i see a PB18 and PB19 lost!!! so. i review the original listing to seek this block. as i suspect this may be a source of the error. also when i iserted the twos modules at plc1 and doing a directory the FB11 not is listed but if i remove the lower module, it il listed in the directory. PB24 make a intesive use of FB11. i try to seek the PB18,19 and load in ram to see the result! Bye and tks juanjo Attachmentplc_alone.zip (259 Downloads) |
Last edited by: juanjoR at: 11/3/2008 2:31 PMLast edited by: juanjoR at: 11/3/2008 11:57 AM |
|
Follow us on