10/15/2019 10:06 AM | |
Posts: 1 Rating:
|
Hello, I'm new in sinamics dcm. I have 6RA80 drive & operating in torque mode using set point as motor potentiometer .During commissioning motor working fine in without load but when i connected load broke SCR in drive. This happened two times.I have attached backup file of program .please help me.. ------------------------------------------------------------------------------------------ AttachmentDrive backup.zip (120 Downloads) |
Last edited by: Jen_Moderator at: 10/15/2019 13:49:26New subject after splitting |
|
10/15/2019 12:07 PM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating:
|
Hello, You should have published this post in SINAMICS product conference. Please provide additional information e.g. mentioned as below. 1. Have you provided SITOR fuses at AC input side of drive as per Siemens recomandations? 2. Which optimisation runs were performed & were followed as per Siemens procedure explained in manual. 3. Have you set motor data correctly? 4. How you are commissioning drive i.e. via BOP or STARTER? |
Follow us on