Industry Online Support
Technical Forum
10/31/2008 12:35 PM | |
Posts: 14 Rating:
|
I need help!! |
11/1/2008 4:32 AM | |
Posts: 2661 Rating:
|
Hi FabioIT, The main difference between your installation and mine is, you don't have Advanced Process Control. But since Danielle also reported that her PCS7 WinCC installation (where APCgets installed automatically)has same problem, I feel it has got something to do with the Windows MUI installation. Check the following: Post Installation of Foreign Languages Under MS Windows XP MultiLanguage Is it possible for you to trywith English or German language installation? For me the tooltip is working in both these languages. If nothing works, I would recommend logging-in a support request with Siemens. Regards |
11/4/2008 8:31 AM | |
Posts: 14 Rating:
|
Yes, This could be a solution, even if in a great project I should insert many images and this isn't simple. Thanks F.Thomè |
11/5/2008 5:00 PM | |
Posts: 14 Rating:
|
Hi, I have just resolved downloading (after support request) Hotfix 10 (for winCC 6.2 without sp2). Thanks!! |
Follow us on